IntraVUE™ Key Performance Indicators
There are 3 Key Performance Indicators (KPI) maintained by IntraVUE™.
- Uptime for critical devices meant to be on all the time
- Total incidents for Devices
- Total Incidents for Switches
Incidents are certain events in the event log such as device disconnects, ip or mac address changes, and over threshold events.
Every device has one of four critical states assigned
- Unknown, the default, means no one has made a determination of this devices state.
- Ignore - the device is not critical to production or operation
- Critical Intermittent - the device is critical but sometimes is not available. For instance a switch inside a robot cell where all power must be removed to the cell before a technician can enter the cell.
- Critical Always On - the device is critical and uptime should be measured and reported.
Ideally, there will be no Critical Unknown devices or only for newly discovered devices.
Refer to for settings location and how to configure them for multiple devices in bulk.
All configuration of the Supervisor is done in the KPI Supervisor Configuration page.