The List View is selected from the KPI drop down menu.
The List View provides a high level summary of each satellite and has columns for data from the satellites. Each column can be sorted in ascending or descending order.
The Name column also contains an icon as described in the previous pages. It relects the icon that is used in the 'combined KPI' view.
'Non Admin Verified' shows the number of devices which are unverified and the total number of devices.
'Unknown Critical Status' shows the number of devices which have not been set to the Ignore, Critical Intermittent, or Critical Always On states, as well as the total devices.
The Critical Device Uptime columns show the current uptime (for the last 24 hours) as well as the lowest and highest percentages for the last 30 days. The Critical Device Count is the count of all devices set to Critical Always On.
The Critical Device Incidents and Critical Switch Incidents section each have several columns.
|