NA Nodes

There are two types of NA Nodes, n/a and N/A and there are subtle differences between them that would help you identify the behavior of each when you see them on the IntraVUE Map View.

 

Auto Inserted n/a Nodes

Ethernet is a point to point protocol. An Ethernet cable can not be physically attached to more than one device at each end.

LAN traffic/packets move based on mac addresses

Switches move packets to ports based on mac address, Hubs move packets to all ports

Fully managed switches report mac addresses on each port

Anytime the scanner detects more than one mac address on the port of a managed switch that can not be resolved to a switch further down on that port, an auto-inserted node will be used to show more than one device on the port – only one line per port from the upper switch

Anytime only one mac is left on a port (because of a device move) the n/a node will be removed

Lower case n/a nodes characteristics

Automatically inserted and removed by the scanner

Only appear on the port of a managed switch

Represents a device which causes the scanner to see more than one mac address on a port of a managed switch

Common examples:

-A hub

-An unmanaged switch (fails to meet RFC 1493 standard)

-A Wireless AP

-A Hypervisor Server

-A DRL Ring (daisy-chained or linear)

 

 

Search for "Device Configuration" and check the option "Virtual Machine, Unmanaged Switch" to device 'X' become the parent of the children in Map View that would replace that 'n/a' node.

 

Manually Inserted Nodes

Upper case N/A nodes characteristics

Manually added by the user

May represent an unmanaged switch

Can show media conversion (copper to fiber and then fiber to copper)

Can show non-IP

 

 

FOR IMMEDIATE SUPPORT CALL +1-800-405-6654 OR EMAIL US AT techsupport@panduit.com

 

Where To Buy: Find a Distributor Near Me