The basic requirements to make use of the IntraVUE Agent are:
-Agent Readiness Checklist. See Installation & Registration
-Agent Configuration. See Appliance Configuration
-Good and stable bandwidth
-Local network access to the automation network (i.e. automation devices can be pinged from this agent).
- Access to the following ports through firewalls:
65402 – used for communication to IntraVUE Agents
65403 – used for communication to IntraVUE Agents
8765 – mandatory port to browse IntraVUE
Additional Requirements for Virtual IntraVUE™ Agents
The IntraVUE Agent also can also be installed in a virtual machine (linux). These are the requirements:
-A hypervisor (V-Spher, ESXi, or compatible)
-2 GB ram OS Ram (4GB recommended)
-64 GB disk space
-Single CPU
-Load the IntraVUE™ agent's image onto a virtual machine using the instructions here http://i-vue.com/vmappliance/
                        
  |